One size does not fit all – some key factors to consider when measuring potable water quality

Jon Penn 25th March 2022
 Jon Penn, 
 Global Product Line Manager - CWA
 Measurement & Analytics  

Share this page

There are many factors that need to be considered when specifying water quality measurement equipment for potable water treatment applications.

While 70 percent of the Earth’s surface is covered in water, over 69 percent of it is unsuitable for human consumption. The less than one percent that is available as readily accessible freshwater must meet the daily needs of a growing population, which is projected to reach around 9.8 billion by 2050. With climate stress adding to the equation, rising consumption will meet decreasing supply, at which point, we simply will not have enough water to supply our needs.

As regulations for water quality become more stringent, added to increasing pressure from customers to provide consistent water quality and rising demand, the water supply industry is continually challenged to optimize water treatment processes with part of that focus being on the testing regimes and how and how often water is analysed.

Low res

Traditionally, testing entailed extracting samples for laboratory analysis and applying the results to the overall performance of the treatment process. Such an approach can only give information for a particular set of conditions at a single moment in time. Because the results are only valid for the time when the test was conducted, the operator is unable to obtain real-time date of their process.  This makes this method inappropriate for today’s demand which now requires raw water to be extracted from multiple sources and blended before treatment.

Continuous Water Analysis (CWA) systems are the best way to meet these needs as they give highly accurate, up to the minute information on conditions.

Whether it’s monitoring influent, used in the treatment stages, or as a final effluent check, an online device can provide continuous measurement, offering several advantages over purely manual methods. With online CWA systems, samples are automatically extracted and analysed at regular intervals without the need for time-consuming and potentially inaccurate manual sample collection

A real-time snapshot of process conditions as they exist also allows operators to take immediate action if any issues occur.

With the added benefit of digital based instruments, CWA systems offer reliable measurement data, are simpler to operate and maintain, and provide flexible communications. Combined with advanced digital predictive maintenance, they can help maintain the quality of drinking water while ensuring that analytic equipment and thus processes remain almost constantly online.

These systems help achieve improvements in treated water quality, increase process efficiency, and reduce use of chemicals and energy, as well as cutting maintenance and personnel costs.

When it comes to water quality measurement in potable water treatment applications, there is no single generic ‘one size fits all’ solution that can be applied in every instance. Instead, the utilization of instruments will vary according to a variety of factors.

Think local

Various local and seasonal conditions and legislation will play a role in the equipment and analysers chosen for the system.

The first stage is to source the water. The two major sources of water are surface water from rivers, streams, lakes and reservoirs, and groundwater from underground sources such as aquifers.

The source of the water is important when building the CWA system, as its geology and geography, vegetation in the area, and human activities determine the initial contaminants. Lowland sources can be contaminated by pesticides and organic matter, while highland or well water sources can have significant quantities of minerals such as iron and manganese. When entering the distribution system, these minerals can cause poor aesthetic quality of the water, or deposition on pipe surfaces. As soluble minerals, they must first be chemically converted to an insoluble form that can be easily filtered out.

Because of this, there are several parameters that need to be measured or considered in the water intake phase of the water treatment process. Some of them depend on the level of other parameters, affecting the makeup of the CWA system that monitors them.

Ammonia can affect the health of animals and people. Its toxicity depends on the pH value of the water as well as the temperature. Generally, the higher the pH value the greater the proportion of ionized ammonia, which increases the toxic effect - raised temperature also increases the proportion of NH4+.

Conductivity is another measurement used in drinking water as an indication of its purity. The level of dissolved ions can change the conductivity of water. In general, the higher the contaminant levels, the greater the conductivity. Measured in microSiemens per centimeter or µS/cm, typical drinking water will be between five and 50µs/cm.

Conductivity also depends on the temperature of the water – as temperature rises, conductivity increases.  This is why measurement of conductivity of a water source is best done in situ, as taking a small sample will alter the temperature and therefore the conductivity value. High conductivity of the order of one to 10 µS/cm could be an indicator that the water source has been affected by industrial processes.

In its natural, pre-treated state, all water contains particulate matter that will need to be removed before it is deemed to be completely safe to drink. The visual appearance of this water can vary depending on its quality and quantity of the suspended particulates.

A sample is turbid when particulate matter in the water makes it cloudy and difficult to see through after a certain distance. Turbidity levels are measured using a turbidimeter, which uses a light beam and a light detector. Turbidity meters are used extensively in water treatment cycle ranging from the measurement of incoming source water, checking the effectiveness of the coagulation and filtrations steps, to monitoring of final effluent prior to distribution ensuring the water is safe to drink and free of potentially harmful microorganisms.

Nitrates, which are another key parameter in drinking water, are found in both ground and surface water usually from agricultural runoff or industrial waste. If present in drinking water beyond a certain threshold, it can be fatal especially for infants. Nitrates are most commonly measured using ultraviolet (UV) spectrophotometry. Nitrates absorb UV light at particular wavelengths giving a rapid way of determining the nitrate content and ensuring the correct mitigations actions can be taken to lower its concentration.

Building the right system

Continuous assessment and real-time dosing of water inputs was the basis of a system designed by ABB for use on a potable water treatment works. The system replaced an obsolete automatic coagulant dosing system that was reaching the end of its life. The customer also wanted improved control and instrumentation to cut OPEX by reducing dosing needs and maintenance effort.

In the initial design stages, the company assessed potential replacement systems and met with other water utilities to compare products and share best practice.

After conducting an initial search, the water company found no readily available solution in the market that met all its requirements. To meets its needs, ABB needed to develop a continuous measurement and control system, combining high and low-range UV organics (DOC), surrogate colour, turbidity and pH analysers with an RVG200 controller/recorder.

The system calculates the amount of coagulant that will allow effective removal of particulates through sedimentation and filtration. Using real-time data from analyzers, the RVG200 adjusts the level of coagulant dosing. This gives values for the actual required dose (mg/l) and dose rate (mls/min), used to ensure that the coagulant accounts for seasonal fluctuations in raw water or physical changes to the process.

The feedback control modifies the coagulant dose by maintaining colour for the clarified water within a set target band. This improved on the previous system that used only feed-forward control.

The system can be adjusted to handle any variations upstream, while using an Ethernet connection enables remote condition monitoring.

After a year of operation, the water company uses 12 percent less coagulant, has cut maintenance by over half, and has reliable control in line with raw water quality changes.

Get the right results

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language