Success story | May, 2020

Shanghai Prosperous Paper’s winder and calender machines are running with Pressductor PillowBlock load cells providing an accurate web tension measurement.

About Shanghai Prosperous Paper

Shanghai Prosperous Paper (SPP) is located in the Baoshan district of Shanghai City and owned by Potential Industries Inc (90 %) and Shi-Dongkou Economic & Trading Co. (10 %). It entered the Chinese newsprint market in 1998 and is known as the garden paper mill because 20 % of its plant grounds are covered by green areas. Based on a business philosophy of “environmental protection, people-oriented”, the company operates a high-speed newsprint line with an annual capacity of 140,000 metric tons. It has been acknowledged as a leading technology enterprise by the Shanghai Government several times.

SPP has stayed with the ABB tension measurement systems since late 1990’s when the mill was built. SPP is very happy with the stable measurement performance of the reliable ABB Pressductor load cells. In general, ABB products have a good reputation and are very trustworthy, leading to a high mill availability.

Screenshot 2024-07-16 114029

What we achieved

We asked Mr Zou Pei Yong, Deputy Section Chief, Electricity/Instrument Section and Mr Sun Quanchang, MaintenanceEngineer, to give us their opinion about the ABB Pressductor load cell installations:

“ABB has a good reputation on the market and we really trust ABB products, for example reliable drives and load cells.”

“The ABB Pressductor load cells have very stable measurements and they are very robust and durable. We are very happy with the ABB tension electronics performance and one good example is that there is never any problems with zero-setting.”

“Now and then, on a regularly basis, we change the load cell positions with each other to see if the load cells have stable measurements and that they measure accurately. The results are excellent every time!”

“SPP is one of the best quality newsprint paper producers in China. There is a stable market for newsprint in China, but we are always working with new product development, one now being interleaving paper for steel plates.

“In the wire section of the machine we are looking for a reliable alternative to today’s wire measurements. ABB load cells, single-side or double-side measurement, might be a good solution.”

ABB's solution 

ABB Force Measurement has supplied Shanghai Prosperous Paper, Shanghai, China with 8 Pressductor PillowBlock load cells.


 

PBT
Shanghai Prosperous Paper
Shanghai Prosperous Paper

Share this page

Discover more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language