Top tips for selecting the right CEMS solution for your business

Time is running short for the world to get its act together on industrial emissions. Recent estimates by the Intergovernmental Panel on Climate Change (IPCC) point to the need for drastic change if we are to stay within the threshold 1.5°C increase in global temperature set by the Paris Climate Agreement in 2016. To achieve this will require a 45 percent reduction in emissions levels from 2010 to be achieved by 2030, with a 100 percent reduction needing to be accomplished by 2050.

Top Tips for selecting the right CEMS solution for your business

The growing need to curb emissions of industrial gases to air has already seen industrial companies being subjected to ever tighter legislation around the quantity and quality of what they emit. The UK has seen a steady improvement in emissions reductions, with levels of key indicators such as sulphur dioxides (SOx), nitrogen oxides (NOx) and non-methane volatile organic compounds (VOCs) having significantly declined compared to 1970 levels. This year, 2020, has seen dramatic photographs of cities once choked on smog with clear skies as industry and transportation shut down in the wake of the pandemic.

Whilst reductions have had an impact, more still needs to be done, especially when it comes to the discharge of other gases such as ammonia, with levels declining much more slowly.

The need to ensure that levels continue to fall places an obligation on industrial operators to monitor emissions as closely and as accurately as possible. This is where continuous emissions monitoring comes in.

Continuous emissions monitoring is crucial to monitoring emissions as closely and as accurately as possible

When it comes to choosing the right emissions measurement solution, there are several key factors that need to be considered

By measuring key parameters such as carbon dioxide, methane and sulphur dioxide, typically in flue or stack gases, continuous emissions monitoring systems, or CEMS, play a key role in helping to keep track of the quality and quantity of emissions from industrial sites. As such, they are a key ingredient in any application where levels need to be measured and reported for regulatory purposes, from power stations through to shipping.

The importance of making the right choice

When it comes to choosing the right emissions measurement solution, there are several key factors that need to be considered. Selecting the right system to be installed, can reduce the likelihood of unforeseen costs from excessive maintenance, through to potential financial penalties for regulatory non-compliance.

To help you make the right choice, we have put together a list of some key pointers:

1. Start with the regulations
With regulations really driving the agenda when it comes to emissions monitoring, it pays to understand what you need to do and how you need to be doing it. Requirements will include the types of gases that need to be measured; which processes require monitoring; how often emissions levels need to be reported; the methods used in reporting and the types of equipment used.

There will also be specific requirements relating to the availability of your monitoring system, which set a maximum number of hours that the equipment can be offline for tasks such as maintenance and checking. Look into certifications or talk to references who can share their experiences about the equipment you are considering. Also ask potential suppliers about calibration and maintenance requirements and how long these will impact the overall availability of the system.

You should also be aware of any local differences in regulations. Different parts of the world have their own specific requirements, making it difficult to apply a one-size-fits-all approach to every application. The EU, for example, operates a certification scheme for analyser systems, whilst the US has a requirement for daily calibration. In the UK, the Environment Agency operates the MCERTS scheme, which sets standards relating to Best Available Techniques and self-certification of analyser systems.

Different parts of the world have their own specific requirements, making it difficult to apply a one-size-fits-all approach to every application

2. The cheapest available solution my be a false economy in the long run

CEMS systems are, by their nature, complex pieces of kit that require specialist knowledge and experience to build and operate properly. Ensure the system delivers the accuracy and reliability needed to guarantees watertight emissions measurement. Failure of these systems can incur financial penalties that outweigh any upfront purchase savings.

Considering that CEMS systems need to work 24/7, there are likely to be instances where even the most reliable unit may need servicing. When this happens, you will need to access to technical support, either remotely or have an engineer on site as quickly as possible with the parts and expertise to fix the problem.

Given these facts, it pays to always look to see which equipment is rated as the Best Available Technique (BAT) for your application, offering reduced ownership costs and ensuring regulatory compliance, as well as the assurance that help and support will be available when and where you need it.

Suppliers offering lower cost solutions are unlikely to be able to provide adequate levels of service and support

3. In-situ or extractive?

While logic might point to having your measurement system located in-situ to get as close as possible to what’s being measured, around 80 to 90 percent of companies would disagree. In most cases, extractive systems – where the sample is removed before measurement takes place – are preferred. There are several reasons for this. 

Firstly, in contrast to in-situ systems, in extractive systems only the probe is in contact with the gas, rather than any delicate optical components that could become damaged and require maintenance. With less to go wrong, the frequency of maintenance, and the attendant cost of parts and servicing, are greatly reduced.

Extractive systems can also measure multiple gas components simultaneously from a single sampling point using a sequence of sensors. This eliminates the requirement for additional holes to be made in the stack to accommodate in-situ devices, which are typically limited to a maximum of two components.

Another benefit is that extractive analyser systems tend to be in cleaner, more accessible locations. This makes them much easier to maintain, with test gas cylinders normally also incorporated to help make calibration easier.

Extractive systems are preferred to ensure lowered maintenance frequency, cost of parts and servicing, to measure multiple gas components simultaneously from a single sampling point and gain higher ease of maintenance

4. Be certain about uncertainty

No measurement installation can ever be guaranteed 100% accurate. While an instrument may well offer the highest levels of accuracy, its ability to measure will be affected by a range of factors, including not just its own design but the design, age and condition of the equipment around it and the way in which the medium is delivered for measurement. The behavior of the medium being measured can also have an impact. The combined impact of all these factors is known as the uncertainty and is factored into the accuracy of all measurement instruments.

In gas analysis applications, ensuring that your analyser can offer the lowest certified measuring ranges give the best indication of required sensitivity at low ppm concentrations. Low cross sensitivities mean your measurement is not influenced by other gases in the sample. Zero and span drift occur when an analyzer‘s performance is not stable, such that low drift equals high quality.

Where the measurement can be affected by changing ambient temperature and pressure conditions, ask your supplier whether the analyser incorporates any compensation functions that can factor them into the final measurement to help iron out any potential errors.

It is crucial to consider compensation functions that factor ambient temperatures and air pressures into final measurement to iron out potential errors

5. Talk to an expert

Lastly, and perhaps most importantly, if in doubt, find an expert to talk to. Manufacturers such as ourselves have extensive experience in all aspects of continuous gas analyser systems, spanning from design through to operation, maintenance and long term support. Using our extensive experience gained through hundreds of applications in multiple industries, we can help you to assess your requirements to make sure that you get a solution that exactly matches your application, whilst avoiding any pitfalls that can occur with less experienced suppliers.  

Got a question? Talk to us

Find out what we can offer and how we can help you to optimize measurement performance whilst minimizing the total cost of ownership by calling us on 0870 600 6122 or emailing us at enquiries.mp.uk@gb.abb.com (ref. 'CEMS selection').

Find out more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language