The pulp and paper industry is in constant innovation mode, and that is great news for sustainability. Customers are not only discovering new opportunities for efficiency and optimization, but also alternatives for resources to reduce emissions. As a partner, ABB is committed to supporting them every step of the way, exploring new ways to help them succeed in lowering carbon.
For example, biomass has proven to be a great alternative source of energy, but recent innovation has seen it also become a very valuable raw material, with some customers refining it into methanol for the aviation industry. Innovation like this is only the beginning as new discoveries are constantly made. At ABB, it’s our role to help customers identify how these can be practically applied with tailored solutions.
I’ve worked with mills who are exploring rice husk and avocado waste as pulp types due to the high cellulose and starch content. Some use bamboo – technically a grass rather than a fiber. On an industry level, we are at the forefront of innovation as a Founding Member of Modellfabrik Papier, a consortium bringing together industry leaders to co-develop technologies that enable carbon-neutral papermaking. As the battle to reduce single use-plastics increases while also developing more sustainable alternatives, ABB are committed to the journey of innovation for our customers and the industry.