ABB Field Information Manager is a software for device management that makes the configuration, commissioning, diagnostics and maintenance of fieldbus instruments easier and quicker than ever before.
Click the button to download the latest version of Field Information Manager.
For usage with ABB Ability System 800xA or Symphony Plus, please consider the specific information below before download.
Operating System Requirements
Field Information Manager Client and/or Server:
- Windows 10 (64 Bit), Windows 11 or alternatively Windows Server 2019, 2022 or 2025.
- 10 GB storage space.
- 1 GB RAM.
Connectivities (Communication Servers and FIM Bridges):
- Windows 10 (64 Bit), Windows 11 or alternatively Windows Server 2019, 2022 or 2025.
- 5 GB storage space.
- 1 GB RAM.
Installation Details
For installing Field Information Manager, please consider the following details:
- Field Information Manager Installer requires administrator rights and guides through the installation process for different application types.
- Standalone installation includes Field Information Manager Server and Client both running on one node, behaving as one application.
- Client/Server installation includes one Field Information Manager Server running on a central node with various Field Information Manager Clients connecting to this server via network (enabling parallel work on the same system).
- Field Information Manager 3.0 or later can be upgraded to the latest version.
- Field Information Manager 2.5 must be upgraded to version 3.0.1 first before upgrading to the latest version. Versions older than 2.5 must be upgraded to version 2.5 first.
Further details in
Field Information Manager - User Guide (7PAA000045*).
Field Information Manager with System 800xA
The following System 800xA versions are supported with FIM Bridge 800xA:
- 6.0.3 (LTS)
- 6.1.1 (LTS)
- 6.2
Further details on ABB FIM Bridge 800xA and the connectivity to System 800xA:
https://new.abb.com/control-systems/fieldbus-solutions/fim/connectivities/system800xa
Please find more information about the supported Windows Server OS versions in
ABB Ability™ System 800xA 6.0.3.4 System Guide Summary (3BSE078159*),
ABB Ability™ System 800xA 6.1.1 System Guide Summary (3BSE091794*) and
ABB Ability™ System 800xA 6.2 System Guide Summary (7PAA007862*).
Field Information Manager with Symphony Plus
For details about Field Information Manager with Symphony Plus, please refer to your ABB sales contact.
Further details on ABB FIM Bridge S+ and the connectivity to Symphony Plus:
https://new.abb.com/control-systems/fieldbus-solutions/fim/connectivities/abb-symphony-plus