Language Support and Language Packs

ABB Field Information Manager Learning Center

In the Language Options the user can change the language of the FIM tools texts and device views. The device views are based on the Device Package information. If the Device Package does not contain the selected language then the default language will be used for the device views.

The default language is English language.

Are you looking for support or purchase information?


Native Support of English and German

A set of the most used languages is part of the FIM installation and the user can select one of these languages. But the FIM installation contains only English and German language completely.

All the other selectable languages require a Language Pack to ensure that all the tool texts are displayed in that language.

Installation of Language Packs

A Language Pack can be installed via drag & drop of the Language Pack file into the tool. An overview of the already installed Language Packs is available via FIM Options - Info page.

Basic Concept

Select region / language