Choose a step-by-step or a complete evolution to System 800xA for ASEA/ABB Master (MasterPiece controller, MasterView HMI) and the Advant Master family (AC450 controller, Advant Station HMI)
Advant Master is a widely installed and supported ABB DCS. A majority of customers have already enhanced their Advant system by adding the System 800xA HMI, AC 800M controller and S800 I/O in order to extend the lifetime of the system and benefit from the latest technologies.
ABB is committed to support our customers with an extensive Product Life Cycle Program to enable you to optimize the life cycle, performance, and the cost to operate your systems
ABB has developed comprehensive solutions with different levels of stepwise evolution for the ABB Master family, introduced as ASEA Master (MasterPiece controller, MasterView HMI) in 1984, and the Advant Master family (AC 450 controller, Advant Station HMI) introduced in 1992.
Our evolution experts offer a complete review of a system in order to identify upgrade opportunities offering the greatest ROI. As a result of the study, a long-term roadmap will suggest the best evolution path to increase the efficiency and the productivity of the plant.