Bluetooth Mesh is a computer mesh networking standard based on Bluetooth Low Energy that allows for many-to-many communication over Bluetooth radio. As a wireless technology standard, Bluetooth transmits data via low-power radio waves.
The Nexus® Pro Bluetooth mesh network operates in the 2.4 GHz ISM band, providing superior penetration through building materials and ensuring network integrity.
Bluetooth mesh uses a technique called spread-spectrum frequency hopping that makes it rare for more than one device to be transmitting on the same frequency at the same time. In this technique, a device will hop between 40 randomly chosen channels, constantly optimizing and changing.
Each mesh packet – piece of data – includes a small identifier that determines which network the mesh packet belongs to. A device in one mesh network cannot decrypt or authenticate packets from another mesh network, and it will never relay those messages. Making each mesh network completely isolated.
ABB will work with you to ensure Nexus®Pro is successfully installed by offering complimentary site evaluations, help select products based on application, photometric calculations, bill of material, and Gateway location placements.
Interested in learning more about Nexus®Pro?