ABB launching sustainable solutions for the water industry at WEFTEC 2025

ABB launching sustainable solutions for the water industry at WEFTEC 2025

Visit ABB at booth 1243, Sep 29-Oct 1 in Chicago

ABB is launching its new Baldor-Reliance SP4 close-coupled pump motor at WEFTEC, September 29 through October 1 at McCormick Place, Chicago, Illinois, U.S. Media is invited to visit booth #1243 to learn how ABB engineered this NEMA Super Premium™ (IE4) efficiency motor with a compact design that simplifies installation, reduces maintenance and ensures reliable performance in demanding pumping applications in the water and wastewater industry.

Like all ABB Baldor-Reliance SP4 motors, the new close-coupled pump configuration reduces motor losses by an average of 20%, compared to standard induction motors, while maintaining the simplicity, form, fit and function of today‘s installed base of AC induction motors. With more than 80% of industrial electric motors operating direct on line (DOL) - without using a drive to improve efficiency - SP4 represents ABB’s commitment to improving efficiency and performance without requiring customers to make significant investments in additional technology or components.

  • Baldor-Reliance SP4 close-coupled pump motor
  • ABB vertical hollow shaft motor
  • Baldor-Reliance SP4 NEMA Super Premium motor
  • Baldor-Reliance submersible pump motor
  • EC Titanium integrated motor drive
  • ABB NEMA Motors SD100 severe duty motor
  • ACQ580 UL Type 4X/IP69 drive
  • ACS880 high-speed drive

Motor and drive solutions on display:

Book a one-on-one interview with an ABB expert here.

ABB Motion, a global leader in motors and drives, is at the core of accelerating a more productive and sustainable future. We innovate and push the boundaries of technology to contribute to energy efficient, decarbonizing and circular solutions for customers, industries and societies. With our digitally enabled drives, motors and services we support our customers and partners to achieve better performance, safety and reliability. To help the world’s industries outrun – leaner and cleaner, we deliver motor-driven solutions for a wide range of applications in all industrial segments. Building on over 140 years of domain expertise in electric powertrains, our more than 22,000 employees across 100 countries learn and improve every day.  new.abb.com/motion

ABB is a global technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. By connecting its engineering and digitalization expertise, ABB helps industries run at high performance, while becoming more efficient, productive and sustainable so they outperform. At ABB, we call this ‘Engineered to Outrun’. The company has over 140 years of history and more than 105,000 employees worldwide. ABB’s shares are listed on the SIX Swiss Exchange (ABBN) and Nasdaq Stockholm (ABB). www.abb.com   

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp