Interview | June, 2025

Dr. Henry Buijs is a pioneer of Fourier Transform Spectroscopy in space science and a co-founder of Bomem Inc., the Canadian company which was acquired by ABB in 1999. Today, ABB’s Quebec City factory is a flagship facility with over 400 employees.

henry-buijs
Henry Buijs who pioneered the FTS technique on SCISAT

Can you tell us about your early involvement with Fourier Transform Spectroscopy and how it impacted the development of spectrometers for use in space?

As a graduate student in the mid-1960s, I became acquainted with the emerging technique of Fourier Transform Spectroscopy. It promised the ability to measure highly detailed spectra with high sensitivity if we could make the interferometers work. Initially, Bomem Inc., the company I co-founded in 1973, flourished by supplying Fourier Transform Spectrometers for investigation of the upper atmosphere by means of balloon-borne solar spectroscopy. This was to determine the reasons for the observed depletion of the ozone layer. We invented a dynamic alignment system to solve the problem of alignment error in scanning interferometers. This ultimately led to the implementation of spectrometers that could achieve a very high degree of absolute accuracy of measurement even for highly complex spectra. This then became the preferred instrumentation for satellites for the measurement of parameters that drive weather conditions.

What were some of the challenges you faced, and how did the team gain confidence from customers?

At first, it was very hard to compete with large aerospace companies in the USA. They believed that they had a unique capability of designing and building reliable satellite sensors - such that they could be shot into space undergoing enormous forces and accelerations and make these subsequently work for long periods of time in orbit. It took us a long time to learn these requirements to the point that customers would have confidence in our ability. In retrospect, we did very well.

Could you describe the significance of the "Atmospheric Chemistry Experiment" mission, and how it contributed to environmental research?

The first of our space instruments designed and built at Bomem was a satellite-based spectrometer for the Canadian government to measure atmospheric chemical composition via solar occultation measurements. The satellite views radiation from the sun as the satellite rises above the Earth, measuring the different gases at different altitudes like a sunrise. Similarly, a short time later it measures the different gases at different altitudes as the sun sets on the satellite. In this way, the satellite measures vertical distributions of atmospheric gases many times each day and located at many different locations on Earth as the satellite passes over. 

The design of this Fourier Transform Spectrometer is unique in that it is the space-based spectrometer with the highest spectral resolution operating in orbit since 2003, quantifying the sun energy transmitted through the Earth atmosphere in over 200,000 different infrared colors every two seconds. The mission is called ACE for "Atmospheric Chemistry Experiment." The satellite was launched in August 2003 and has operated flawlessly and uninterrupted for the last almost 22 years. It is recording precisely the steady rise or decrease of over 46 different gases in our atmosphere, some present at incredibly low concentration, many of which are related to human activities. The data obtained by this satellite continues to play an important role in regulating the worldwide uses of various refrigerants that have been identified as responsible for affecting the ozone layer.

Recently, scientists expressed concern regarding the possible loss of monitoring capability from orbit with the termination of long-lived science missions. In a detailed paper, they point out that ACE along with the Microwave Limb Sounder (MLS) instrument on the NASA Aura satellite mission (set for termination soon) are the only two instruments capable of measuring changes to stratospheric composition which influence our climate.

infrared-fourier-transform-spectrometer
The infrared Fourier Transform Spectrometer is able to distinguish 200 000 different infrared colors
The scientists point out that the original requirement for ACE was to complete a two-year mission and that it currently exceeds the mission objective more than 10x times. But this could end at any time without warning. To date, there are no indications of any appreciable degradations in operation but a collision with space debris or fault with aging electronics could end the mission abruptly in unrecoverable fashion.

There is a strong need for planning follow-up missions to ensure continuity of the capability to measure climate change from space.
scisat-mission
The Canadian Space Agency’s SCISAT mission

How did you get into building instrumentation for weather-related missions?

We were fortunate in early-on becoming acquainted with researchers at the University of Wisconsin who were interested in developing newer and more performant instruments for weather satellites. We worked with the team under the leadership of Professor Suomi at the University of Wisconsin - historically the father of weather satellites. We supplied a spectrometer to carry out tests of weather prediction mounted under the wing of a U2 aircraft. This program of flying over specific weather systems at high altitude continues even today. The University of Wisconsin’s program developed the specifications for a new next generation satellite-based sounder which they based on our spectrometer technology. This is how we became the developer and supplier of the "Cris" infrared radiometer for the next generation US weather satellite program and eventually the Himawari-10 mission.

Can you tell us about your work on the GOSAT project for the Japanese Space Agency?

My colleague Marc-Andre Soucy and I travelled to Japan many times to convince the Japanese Environment Agency and the Japanese Space Agency to award us the contract for the spectrometer to be sent in orbit on the Japanese GOSAT mission. It was a steep learning curve for the Japanese as well as for us. The Japanese were interested in measuring the global concentrations of carbon dioxide and methane by means of solar radiation reflected from the Earth surface.

To calibrate these concentrations, we included the short wavelength oxygen, a band in the measurements. In addition, since our Japanese partners had a good quality cryogenically cooled longwave infrared detector, they asked us to include the thermal infrared spectral region as well. This was quite a challenge, requiring a Fourier Transform Spectrometer that could cover an extraordinarily wide spectral range from the visible spectrum all the way to the thermal infrared. Could we do this? We worked out the design of a Fourier Transform Spectrometer with a very wide spectral range – something that had not been done before.

After building the spectrometer we also assisted the Japanese Space Agency with the integration and testing of the system in the satellite configuration. In the end we did very well, and the satellite was launched in January 2009.

Because of the very wide spectral range of the spectrometer of GOSAT 1, a surprising discovery was made. Near the spectral region of the oxygen A band near the visible part of the spectrum, the GOSAT 1 instrument measured a change in signal intensity when passing over areas on the globe with growing vegetation. This has been attributed to a fluorescence signal given off by healthy plant growth. Since its discovery it has become a valuable indicator of the global health of plant growth which is actually an absorber of carbon dioxide and hence positively affects the state of global greenhouse gases.
“The Fourier Transform Spectrometer can sense 70 different molecules and their isotope variants down to parts per trillion, more than any other satellite currently in orbit.”

 

Award-winning ozone chemistry project

In 2009, the Canadian Aeronautics and Space Institute bestowed the Alouette Award to the team behind the "Atmospheric Chemistry Experiment" for outstanding contributions to advancement in Canadian space technology, applications, science, and engineering.

In 2005, Dr. Henry Buijs received Les Prix du Québec from the Government of Quebec, an award given to individuals for their cultural and scientific achievements. In 2011, he was awarded the John H. Chapman Award by the Canadian Space Agency for his outstanding contribution to the Canadian space program.

Today, ABB applies its vast expertise acquired in earlier high-profile government space missions to the private sector space with a focus on actionable low latency satellite data for civil uses.

Share this page

Discover more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language