Blog_banner_under-pressure-managing-water-network_1200x300

Under pressure: Managing water networks with effective pressure management techniques

Krishna_Prashanth_120x120

Opinion | March 22, 2023

 

Krishna Prashanth

Global Product Line Manager, Electromagnetic Flow Meters

 

Growing water scarcity drives the need for effective demand management in water utilities across the world. Pressure management can be viewed as a form of demand and leakage management. Here’s why. 

Water network management is a critical component of providing safe and reliable water supply to communities around the world. Pressure management and flow measurement are two critical components of water network management that are essential for efficient and sustainable distribution of water resources. 

Pressure management is the process of regulating water pressure in water networks to ensure efficient and sustainable distribution of water. High water pressure can lead to increased water demand, particularly in areas with high population densities, making it difficult for water utilities to meet the demand, resulting in supply shortages and water shortages. Pressure management is essential in controlling demand in such situations. By reducing the water pressure, the demand for water can be effectively controlled, resulting in a more efficient and sustainable distribution of water. 

In addition to controlling water demand, pressure management also plays a critical role in reducing water leakage. Water leakage is a significant problem in many water networks, resulting in the loss of treated water due to leaks in some networks. High water pressure can cause pipes and fittings to fail, resulting in leaks. By reducing the water pressure, pressure management can significantly reduce water leakage and the associated economic and environmental costs. 

Effective pressure management requires the use of pressure-reducing valves (PRVs), which are installed at strategic points in the water network to regulate water pressure. The use of modern technology such as flow sensors and telemetry can help to optimize pressure management and improve efficiency. 

The ABB AquaMaster and pressure management

The ABB AquaMaster electromagnetic flowmeter is a state-of-the-art technology designed for accurate and reliable flow measurement in water networks. The instrument has no moving parts, making it suitable for use in harsh environments. The use of pressure input in conjunction with electromagnetic flow measurement technology allows for improved accuracy in flow measurement. Pressure sensors are placed upstream and downstream of the flow meter, allowing the instrument to compensate for changes in pressure and temperature. This compensation ensures that the flow measurement is not affected by changes in pressure or temperature, resulting in more accurate measurements. 

The AquaMaster electromagnetic flowmeter with pressure input can be used for a variety of applications in water network management. For example, it can be used for measuring the flow of water in pipelines, distribution networks, and reservoirs. The instrument can also be used for leak detection, water balance calculations, and pressure management. 

Blog_image_abb-aquamaster_600x450

One of the main benefits of using AquaMaster electromagnetic flow measurement with pressure input is improved accuracy in flow measurement. The instrument can provide accurate measurements even in difficult flow conditions such as low flow rates, high flow velocities, and pulsating flows. This accuracy is essential for water network management, where accurate flow measurement is critical for effective distribution and management of water resources. 

Another benefit of using AquaMaster electromagnetic flow measurement with pressure input is improved efficiency in water network management. The instrument can provide real-time flow measurement data, allowing water utilities to monitor and manage their networks more effectively. The instrument can also be integrated with other monitoring and control systems, such as SCADA (Supervisory Control and Data Acquisition) systems, to provide a comprehensive water network management solution. 

The AquaMaster electromagnetic flowmeter with pressure input is also easy to install and maintain. The instrument has no moving parts, reducing the need for maintenance and calibration. It also has a long lifespan, reducing the need for replacement and ensuring long-term reliability. 

In conclusion, pressure management and flow measurement are critical components of water network management. The use of pressure management and AquaMaster electromagnetic flow measurement with pressure input is an effective method for improving water network management. Pressure management is essential in controlling water demand and reducing water leakage. AquaMaster electromagnetic flow measurement with pressure input provides accurate flow measurement and improved efficiency in water network management. These technologies are essential for ensuring the efficient and sustainable distribution of water resources to communities around the world. 

Read more about AquaMaster

Share this page

Discover more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language