But there’s a catch. During production cycles, the temperature of lubricating oil fluctuates – usually upward. And since density is temperature-dependent, raw readings taken at process temperature can be misleading or even meaningless when compared over time.
To make sense of the data, engineers need a consistent baseline. That’s why API Density at reference temperature is the industry standard.
It helps normalize the measurement, stripping out the noise introduced by temperature swings, which leads to media change, and allows for accurate trend analysis.
Note: API Density is always referenced to a standard temperature. While this blog refers to the value at a reference temperature of 15 °C, it's essential to note that this reference can vary by region – for example, 60 °F (15.56 °C) in the US, or even 20 °C in some other countries.