How to implement Internet of Things, Services and People in industrial environment based on 800xA control system

ABB's System 800xA offers the shortest and most secure path to the realization of the benefits of Internet of Things within process automation. Solving actual problems at your plant and achieving real business benefits in a cost-effective way.

このページをシェアする

800xA-and-the-Internet-of-Things-Large.fw

Low-cost sensors and internet connection drive new decision making models in the industrial domain

The industry trend is smarter devices with software based services exploiting the increased connectivity, bandwidth, computational capabilities and power efficiency, combined with the scalability and cost advantages of cloud computing. In 800xA this is the element the empower collaboration within and between plants, among people, system services and devices. All enabled by the use of the devices, the so called Internet of Things (IoT), as collaboration hubs. This forms the foundation for the information sharing, between People, Systems and Things, required to improve decision making and automation for optimal productivity now and in the future.

There are many services in industrial plants, transforming processing and manufacturing, e.g. collecting large quantities of device data for subsequent (big) data analytics to support predictive maintenance. It is also possible to envision the big data analytics as part of closed control loops, and act based on the analytic information in real-time.

It is also possible to envision the analytics as part of control loops, and act on the information in real-time.

Implementation challenges in critical industrial applications

There are similarities between IoT for general systems and industrial systems, but with respect to scalability, there are also significant differences such as constraints on low latencies, criticality of the systems, requirements for predictability,  resilience to failures in the system and cyber security. Hence, there is justification for specifically consider industrial IoT systems (industrial Internet, Industry 4.0). Including humans in this scenario ABB talks about “Internet of Things, Services and People (IoTSP)”.

Clearly, there are challenges that need to be addressed to support critical industrial applications in an industrial internet scenario.

Industrial internet faces constraints on low latencies, mixed criticality of the systems, requirements for predictability, resilience to failures in the system and cyber security

Examples of IoTSP implementation challenges within process automation that needs to be addressed

  • Resource management related to edge computations, e.g., allocation of computations at different infrastructure levels ranging from edge (field or shop floor) to cloud.
  • Architectures for robust and predictable control in an Industrial IoT setting.
  • Supporting heterogeneous network technologies including Ethernet based field busses through virtualization techniques.
  • Analysis framework for servers, communication, distributed systems for applications spanning in several levels of the IoT infrastructure.
  • Runtime adaptable mechanisms for optimizing resource usage or for fault tolerance management in the IoT infrastructure.

Control system reimagined to play a new role

Industrial automation technology, with more emphasis on information, is the safest and most secure platform to  implement and operate  the Internet of  Things, Services and People in industrial applications. Over the past 10 years, ABB has been on the leading edge for IoT concepts, by reimagining and transforming its 800xA control system  to play a new role in more and more instrumented and connected world.

For 800xA we see it as our mission to continuously improve the collaboration between people, systems and equipment in and between plants.


There are many IoTSP related activities that will result in new functions and systems that will help us in this mission. As these concepts evolve and become reality we feel that we are very well prepared to take advantage of these to further improve our customer offering.

800xA offers safe and secure technology to implement and operate Internet of Things, Services and People in industrial applications

Move over to new functionalities - smoothly

With ABB Aspect Object technology, our IoT technology, we have an infrastructure that allows us to easily attach new functions as well as replace existing functionality with new - all without changing the way things work for our users.

One example of this is how we moved from one graphics engine to a new engine by first allowing both running in parallel and then smoothly moving customers over to the new.

Connect the unconnected - seamlessly

Another example is how we connect to PLCs, controllers and ERP of different brands. 800xA has a unique cyber-physical representation of the equipment in the plant - the Aspects object, the Things in our system.

In 800xA users can enjoy the power of having their equipment seamlessly collaborating with maintenance and video surveillance systems, even if the equipment is not controlled by ABB controllers.

Internet of Things, Services and People will definitely bring new types of equipment and systems into collaboration with our users.
800xA users can enjoy the power of having their equipment seamlessly collaborating with maintenance and video surveillance systems, even if not controlled by ABB controllers

Operate industrial internet - securely

Security remains the foundation for building future industrial systems based on Internet of Things, Services and People, as they are particularly exposed to physical and cyber security risks. System 800xA has the most advanced defense mechanisms in place to operate modern plants, as they move to the higher level of connectedness, mobility and networking.

Act on collected data - collaboratively

Contextual understanding of the data obtained from connected devices is the key element in adding business value from the IoTSP. Having information available is not helpful unless it can be acted on in a timely fashion. This could mean distributing it to individuals inside the organization, other systems in the network, other devices, or back to the device itself.

No context to the data means that we end up with a big mess (instead of big data), and the analytics can deliver the wrong result (that may look right). With mobility we can put wrong information in front of many people, quickly.

The Aspect object technology makes sure that all data is put into the right context and by this we avoid losing track of the information.

ABB has deep understanding of how everything works in industrial environment, in most complex processes. We have the expertise, infrastructure and models to transform the data into actionable information, to help our customers interpret the information and drive optimization. The optimization can be either localized or systematic, and it can be manual or automated. All connected devices, systems and people need to operate in concert with each other.

We have the expertise, infrastructure and models to transform the data into actionable information, help our customers interpret the information and drive optimization.

The keys to making the IoTSP successful in the long run are the intelligent assets, security, contextual data, and a business problem to solve. The good news is that ABB has been addressing these areas for years, and remains your reliable partner at the forefront of the IoT wave.


Deploying the IoT technology

  • お問い合わせ

    ご質問内容などをご入力の上、お送りください。 担当者より折り返しご連絡いたします。

    お問い合わせ
Select region / language