ABB, committed to transferring know-how to the Greek market for the production of high quality standardized Medium Voltage panels, created a program so that the partners who completed the necessary training, which included:
ABB designs analysis
production of samples complying with IEC 62271-1 and IEC 62271-200 standards
running all the necessary tests required by the international standards, and
the audit of the internal procedures and production facilities for the production of UniSec panels in accordance with ABB requirements
have been granted the production license, as well as the permission to use the above UniSec logo for commercial use.
The necessary investment which the network of our certified partners has made, in the aspect of both the configuration of the production facilities to meet the necessary requirements, as well as the essential equipment required for the panels manufacture and the training of their human resources, ensures the quality and high standards of the final product.