ABB GMDs make remote mines and low ore grades economical and transition mills to digital operation

Share this page

What solutions are powering forward the new copper miners, making low ore grades economical to grind? Which mills have made most progress in transitioning to digital operations? Gearless mill drives (GMDs) offer ore producers unrivalled availability, efficiency and durability, while reducing operating expenditure and taking advantage of digitalization.

GMD hero
To take full advantage of the internet of things, it is necessary to have a system that supports a flexible, scalable and reliable cloud platform with a range of comprehensive services protecting your plant regardless of location.

GMD - best solution for driving larger, powerful grinding mills

Larger ball and SAG mills, with higher installed power ratings relative to the mill diameter, offer higher efficiency and throughput, round-the-clock reliability and the opportunity to mine in remote areas. This makes low ore grades economical to grind. Whether it is size or an installation at the highest altitude (4600 m.a.s.l.), gearless mill drives (GMDs) are well positioned to contribute to the building of larger and ever more powerful mills.

GMDs are the grinding solution of choice in challenging environments like high altitudes or varied climates in remote locations. By eliminating bolt-on mechanical components such as ring-gears, pinions, couplings and gearboxes, GMDs offer ore producers unrivalled availability, efficiency and durability, while reducing operating expenditure.

Both ring-geared mill drives and GMDs can be employed to drive autogenous, semi-autogenous (SAG) and/or ball mills. The applications may be the same, but the challenge now is to develop bigger drivetrains with the power to drive these larger grinding mills – and this is exactly where GMDs come into their own.
Whether it is size or an installation at the highest altitude (4600 m.a.s.l.), gearless mill drives (GMDs) are well positioned to contribute to the building of larger and ever more powerful mills.

Highest power, availability and energy savings up to 3%

Unlike more traditional ring-geared mill drives – where a ring-shaped gear encircles the mill and drives it through one or two pinions followed by conventional motors – GMDs work by mounting rotor poles directly to the mill body and surrounding it with the stator ring, meaning the mill itself is incorporated into the motor.

The necessary torque to turn the mill is transmitted between the GMD motor and the mill via the magnetic field in the tiny air gap between the stator and rotor. Because this type of motor system requires no gearing or direct contact transmission, GMDs boost efficiency by reducing frictional losses, while fewer mechanical critical components means less maintenance downtime is required due to wear and tear, according to ABB.

GMDs offer the highest power and availability compared to other driving methods.Efficiency gains are possible by eliminating mechanical components that may fail and add unexpected and costly bottlenecks in the production process.

ABB GMDs use a high efficiency cycloconverter to drive the motor. The same efficiency applies to other system components like transformers and the motor control centres incorporated into ABB’s E-house solution called Control Block; together, these advancements can boost energy optimization in grinding mills by as much as 3%.

That equates to a significant amount of money saved, especially when you consider that some modern mines may have as many as six 15–25 MW GMDs running in parallel.

CASE STUDY

Commercial production of copper now underway at large open pit Cobre Panama mine

When you consider that some modern mines may have as many as six 15–25 MW GMDs running in parallel, 3% energy optimization equates to a significant amount of money saved
ABB successfully commissions six gearless mill drives at Panama's newest mine
The six ABB GMDs, which are the most powerful mill drive systems on the market are all now in continuous operation. Two 28 MW gearless mill drive systems (GMDs) are operating in the mine's 40 foot SAG mills and four 16.5 MW GMDS are employed in 26 football mills along with associated control systems.

Digitalization bringing visualisation and transparency

Advancements in big data, and digital technologies such as the industrial internet of things, the cloud, data analytics, artificial intelligence and advanced modelling algorithms now offer mining companies unprecedented visualisation and transparency along the entire mine production chain, enabling them to carry out predictive rather than reactive maintenance operations from remote locations.

Using the ABB Ability™ cloud platform, GMD operators can access key system parameters, gathering and collating real-time data from sensors in the system, everything from insulation monitoring to status of the air gap to the temperature of rotor poles and stator windings.

Every hour of unplanned shutdown in a mine can cost the operator hundreds of thousands of dollars. Predicting when key parameters will reach critical levels and halt production is, therefore, crucial.

Using data sets collected from the GMD that are processed by specialised algorithms in the ABB Ability Cloud platform, together with ABB engineers, critical situations can be predicted and then timely notify customers in advance, avoiding costly downtimes.

GMD operators can access key system parameters, gathering and collating real-time data from sensors in the system, everything from insulation monitoring to status of the air gap to the temperature of rotor poles and stator windings
CASE STUDY

Example of predictive notification in action

The system alerted us to the fact that there was an anomaly in the air gap between the rotor and the stator. The ABB Ability predictive maintenance system sent an automatically generated SMS and email to the customer and to ABB’s lifecycle manager advising them to check it. They stopped the machine and found a small nut in the air gap that could have scratched the insulation and maybe even caused something more serious. An investigation followed as to identify why the nut was there in the first place and the most plausible cause was that somebody accidentally dropped it while inspecting the machine.

We have reports from customers that almost 100 hours of downtime have been avoided by using this proactive approach to servicing.
Almost 100 hours of downtime have been avoided by using this proactive approach to servicing

No compromise in availability

All this is only possible if the machine has the right instrumentation in place.


Much like a passenger airplane, GMDs are equipped with dozens of sensors to protect it and help the operators to run it smoothly. ABB makes no compromise in its availability-centered design. Our focus is not to eliminate critical protection components of the system to cut costs. We want to give operators peace of mind and allow them to embark on the 4th Industrial Revolution. This is only possible if we have the right instrumentation in place as well as a robust condition monitoring system.

To date, ABB has the capability to remotely support over 100 mills in operation, while over 30 of them are already benefiting from our ABB Ability predictive maintenance platform.

CASE STUDY

Examples of how remote services prevented many hours of production losses

ABB has the capability to remotely support over 100 mills in operation

Optimizing grinding controls

A milling circuit is a complex, multi-variable interacting system. Dynamically changing ore conditions and wear parameters pose particular problems for grinding controllers. By integrating data, the automation system optimizes grinding controls, avoiding the need for constant manual tuning. Feed-forward data on ore quality and quantity, rock face production rates or market demand rates can be used to optimize the grinding stage.
CASE STUDY

Detecting changes to ore grade as it is extracted and optimization using real time data

The typical results of advanced process control are increased throughput, homogeneous product quality and lower maintenance costs.


Improving insulation and preventing moisture ingress

Water and moisture ingress can potentially be a significant issue in ring motors, especially at sites with high levels of precipitation and humidity. In 2005, ABB modified its insulation system and, more than 100 machine years and 6 million operating hours later, no major problems have been reported.

Our heat exchangers – located in the cooling box structure – are solely installed on the bottom of the motor, for example, meaning there is no risk of water ingress elsewhere, whereas in non-ABB GMD designs the cooling boxes are placed around the stator, increasing the risk of water leakage.

We also use leak detection instrumentation in the cooling boxes, humidity and air temperature sensors, differential pressure transmitters and flow meters to detect any leak due to any changes in these parameters.

Our single-bar winding design concept allows for full continuous vacuum pressure impregnated insulation. We can also employ online partial discharge monitoring, especially when the mine is situated in high altitude areas, such as in Chile and Peru.

CASE STUDY

Aktogay and Bozshakol copper mines in Kazakhstan expected to process 25 Mt/y of ore.

KAZ-Minerals-GMD
Each includes phase and excitation transformers, a ring motor with a local mill control panel, and a containerized electrical house (E-house) including cycloconverter and advanced specific grinding control software
ABB was awarded a multi-million contract to provide a 28 MW GMD for a 40 ft (12.2 m) SAG mill and two 22 MW drives for a pair of 28 ft (8.5 m) ball mills at Aktogay, and three identical systems at Bozshakol

Expanding existing mining operations

It obviously costs operators less in terms of capital expenditure to expand existing operations rather than build a new mine, and we have added more digital streaming capabilities to these new GMDs.
Aktogay
We are currently working on the expansion of Aktogay, which aims to double its capacity. ABB will install an additional 40 ft, 28 MW SAG mill and two 28 ft, 22 MW ball mills to the project in order to meet the challenge of higher-capacity production coupled with low ore grades.

Learn more

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language