DCS Modernization without Disruption

Future-proof your Operations

Select Language
  • English
  • Deutsch
  • italiano
  • magyar
  • français
  • polski
  • español
  • čeština
  • Ελληνικά
  • Nederlands (België)
  • Türkçe

Modernizing Distributed Control Systems (DCS) is essential for industries aiming to enhance operational efficiency, reduce downtime, ensure cyber security and stay competitive in a rapidly evolving technological landscape. This page will guide you through the importance, approaches, and benefits of DCS modernization, ensuring your systems are future-proof and aligned with industry standards.

Interested in DCS modernization?

Get in touch with our experts.

Why modernize?

Many industrial manufacturers today have aging DCS currently in place. These legacy systems may work fine today, yet as time goes on, there is increased potential for exposure to a variety of risks which may prevent you from capitalizing on productivity benefits from state-of-the-art technologies.

ARC whitepaper on “The Strategic Imperative of Modernizing Control Systems”

Download

Key reasons to modernize

lifecycle-costs-modernization-dcs
Lower life cycle costs & boost reliability

Aging systems drive up maintenance costs and increase the risk of unplanned downtime. Modernizing control systems reduces total cost of ownership by improving uptime, minimizing emergency repairs, and extending asset life.

digitalization-modernization-dcs
Enable digitalization & data-driven decisions

Modernized systems unlock real-time data, predictive maintenance, and seamless integration with enterprise platforms. This is the foundation for Industry 4.0 and smarter, more agile operations.

How to future-proof your OT systems against rising cyberattacks

Learn now

Approaches to modernization

When modernizing a Distributed Control System (DCS), two primary strategies are available: 
Stepwise modernization
Rip and replace
Also known as systematic replacement. ABB’s preferred approach to help customer with gradual upgrades aligned with their planned maintenance windows, while preserving IP in existing infrastructure like I/O modules and cabinets and introducing new capabilities incrementally.

Benefits:

  • Minimized downtime: Gradual upgrades reduce the need for extended shutdowns.
  • Cost-effective: Phased implementation spreads out costs over time.
  • Enhanced flexibility: Allows for customization and adaptation to specific operational needs.
  • Risk mitigation: Reduces the risk associated with large-scale system overhauls.

Considerations:

  • Longer implementation time: The process may take longer to complete compared to a full replacement.
  • Complex coordination: Requires careful planning and coordination to ensure seamless integration.
  • Potential compatibility issues: May face challenges in integrating new components with existing systems.

 

This method involves a full system overhaul by removing all legacy components and installing a new DCS from scratch. It is a more radical approach but can be effective in plant requiring major infrastructure upgrades or where legacy systems are obsolete and unsupported

Benefits:

  • Complete overhaul: Provides a fresh start with the latest technology and features.
  • Uniformity: Ensures all components are up-to-date and compatible.
  • Potential for innovation: Allows for the implementation of the latest innovations without constraints from legacy systems.

Considerations:

  • High initial cost: Significant investment required for new equipment and installation.
  • Extended downtime: Requires a complete shutdown of operations during the transition.
  • Risk of disruption: Higher risk of operational disruption during the changeover.

 

ABB’s stepwise modernization approach

ABB’s modernization strategy is rooted in “Innovation with Continuity”; a phased approach that minimizes disruption while enabling continuous improvement. Instead of overhauling your entire system, ABB introduces new features and upgrades incrementally, aligned with your plant’s lifecycle and budget. Once on the latest supported version of ABB’s DCS, customers can take advantage of its modular architecture and built-in flexibility to modernize continuously—without waiting for major shutdowns.

ABB enables this through:
  • Support for mixed system environments: ABB maintains flexibility in mixed control system environments by leveraging the existing interoperability of ABB's control systems and through phased evolution without needing disruptive replacements.
  • ABB Adaptive Execution™, a digitally enabled methodology that combines early-stage collaboration, standardized workflows, and modular execution. This reduces cost, mitigates risk, and keeps projects on schedule.
  • Modernization tools for both ABB and third-party systems, ensuring the IP is transferred into the most recent libraries.
  • Sustainable reuse or retrofitting of existing infrastructure, whether it be field wiring, I/O modules, or cabinets.
  • Global Capability Centers in Bangalore, Czech Republic, and Argentina, with dedicated teams specialized in DCS evolution and hardware upgrades, to support local delivery teams.
  • Qualified channel partners with proven experience in ABB’s Control System modernization.

Each step in ABB’s stepwise modernization approach is designed to align with your plant’s life cycle planning and maintenance schedule, ensuring the modernization process is low-risk, customer-paced, and future-ready. You will be able to enjoy the benefits of digitalization and augmented operations, enabling them to face the changing scenarios with more resilience.

Benefits of modernization with ABB

Modernizing your Distributed Control System (DCS) shouldn't mean shutting down production. ABB’s stepwise approach allows you to upgrade legacy systems step-by-step; preserving your intellectual property and field wiring while unlocking the power of modern automation, AI, and advanced cyber security.

refining_picto
Operational resilience

ABB's stepwise modernization approach keeps operations running while putting customer needs first.

Sustainable Energy Optimization
Energy efficiency & sustainability

ABB reuses existing infrastructure where possible, while modernized systems cut waste, lower energy use, and enhance product quality.

Mixed systems support
Mixed systems support

Retain the flexibility of your mixed system environment

digital-and-ai-icon
Enhanced digital capabilities

ABB's modernization solutions unlock digital capabilities, paving the way for integrated, data-driven, and AI-enhanced operations that improve decision-making and responsiveness.

compliance-icon
Compliance & regulatory readiness

Ensuring safety, financial, and environmental compliance.

co-creation-icon
Flexible engagement options

Modernize your control systems directly with ABB experts or through our network of authorized channel partners.

high-voltage-substation-teaser

Seamless evolution for ABB's Harmony Rack installations

Harmony Rack has powered utility automation worldwide. Now, future-proof your current infrastructure with Symphony® Plus SDe with a more sustainable and cost-effective strategy. ABB's stepwise evolution approach enables incremental upgrades with minimal disruption, preserving wiring and hardware while evolving your automation technology. Protect your investment and modernize with confidence. 

FAQ about DCS Modernization

The following FAQs describe how ABB supports step wise DCS modernization while minimizing operational risk.

Getting started

  1. How can we modernize without stopping production?

    DCS modernization can be implemented using a stepwise approach that upgrades selected system components within planned maintenance outages. This minimizes operational disruption, avoids major shutdowns and protects investments in the DCS.

  2. Can DCS modernization be done without a full system replacement?

    It depends on the control system in question. If the system is still supported, modernization would not require a full “rip-and-replace” of the control system.

    ABB’s “innovation with continuity” principle supports phased, stepwise modernization i.e. gradual upgrades of individual components; such as operator workstations, servers, engineering tools or controllers, while ensuring operation continues smoothly.

  3. Is my legacy DCS obsolete? 

    Obsolescence is contingent upon both the control system and its version. The term "legacy" may refer to outdated control systems for which hardware upgrades and software updates are no longer supported. Conversely, it is possible for modern control systems to operate on obsolete hardware or outdated software versions. In both cases, the risk of unexpected downtime increases.

    ABB’s modernization focuses on prioritizing and addressing current needs such as cyber security, data access, regulatory compliance and long-term support, while retaining or retrofitting functioning infrastructure or equipment wherever feasible.

ABB systems & people impact

  1. Do modern control systems, like 800xA, Symphony Plus or Freelance systems require modernization?

    Even modern DCS platforms can require modernization over their life cycle, due to evolving cyber security threats, regulatory requirements, and changing industrial priorities. ABB’s “Innovation with Continuity” principle supports continuous modernization within the systems - 800xA, Symphony Plus, and Freelance, to move to the latest version. It helps plants to manage updates and stay current with supported software versions and capabilities. This approach reduces operational and cyber security risk, while also unlocking the latest system enhancements.

  2. Can we modernize while keeping our operators productive?

    Operator productivity can be maintained during modernization by upgrading operator interfaces gradually while preserving familiar workflows. Some modernization activities require operator support. Training during planned shutdowns and change management support a smooth transition for operations staff.

Risk, cybersecurity & execution

  1. How does DCS modernization reduce operational risk?

    Operational risk can be reduced through phased implementation, controlled migrations, parallel testing, and rollback strategies. Modernization upgrades systems to the latest supported software and hardware, ensuring easy access to parts and expertise. New engineers and operators, often trained in current technologies, find it easier to onboard to modern control systems, reducing reliance on legacy knowledge.

    ABB applies a stepwise modernization approach, proven engineering methodologies and dedicated modernization tools to protect the IP and manage change while maintaining plant safety and availability.
     
  2. How does DCS modernization improve cyber security?

    Modern DCS platforms support defense-in-depth architectures, secure patching, access control, and compliance with current cyber security standards such as IEC 62443. ABB’s modernization programs incorporate these capabilities to help close security gaps common in heritage control systems.

Value & lifecycle confidence

  1. What happens to existing communications,  field wiring and field instruments?

    In most cases, existing communication, field wiring and field instruments can be retained during DCS modernization. Modernization projects can also include field wiring and field instruments to replace aging hardware or to upgrade capabilities.
     
    ABB designs modernization projects to reuse these assets wherever possible, reducing engineering effort, project risk and risk of extended outage duration for rewiring and testing.

  2. What is the ROI beyond system reliability?

    Beyond reliability, modernization delivers benefits such as reduced maintenance effort, compliance with local regulations, unlocks data for AI/ML and digital applications, reduces energy consumption and closes cyber security gaps that legacy, outdated versions of systems cannot address.

  3. How do you ensure long‑term support after modernization?

    Maintenance contracts that cover life cycle services, software support agreements, and obsolescence management help ensure the system remains supported, secure, and upgradeable over time.

    ABB Care service contracts cover DCS life cycle services, including security, parts, and asset management. Through automation software maintenance programs in ABB Care, control systems can be supported and upgraded through the lifetime of the plant.

More FAQs

  1. How long does a typical DCS modernization take?

    Timelines vary depending on scope and plant complexity. A phased approach spreads HMI, controller, and I/O upgrades over time, avoiding a single high-risk cutover and allowing benefits to be realized incrementally.

    ABB helps to plan stepwise modernization projects that occur during scheduled maintenance outages, reducing time to cut over. Read some modernization customer stories here
     
  2. What is the impact on plant safety and availability?

    Modernization improves system reliability, diagnostics, and redundancy, supporting plant safety and availability. Improved visibility and system health monitoring enable safer and more predictable operations.

  3. Can modernization be aligned with future expansions?

    Modernizing the control system establishes a foundation for future expansion by increasing its capacity and scale to accommodate digital and AI technologies. A stepwise modernization roadmap is designed to support incremental future capacity increases, new process units, or technology additions, avoiding repeated reengineering of the control system. Read more about ABB’s Automation Extended program here

  4. How does DCS modernization support digitalization and AI use cases?

    Modern control systems provide structured, high-quality data that can be used for advanced analytics, asset performance management, and AI-driven optimization; capabilities that are difficult to achieve with outdated system architectures. By modernizing their DCS, industries gain access to edge technology and the Industrial Internet of Things (IIOT), preparing them to take advantage of digital and AI capabilities.
     
  5. What if we are not ready to modernize everything at once?

    That is expected. Most organizations prefer to modernize in phases rather than all at once, allowing them to manage projects around downtime and budgets. This approach spreads investments and reduces risks by upgrading over several years.
     
    ABB designs flexible modernization roadmaps specific to each system, or mixed systems environment, that can be adapted to budget cycles, operational priorities and risk appetites, allowing plants to modernize at their own pace.

  6. What is the impact on plant safety and availability?

    To ensure DCS remains compliant with ever-changing safety standards and industry norms, it is essential to modernize control systems. Aging electronic components can undermine plant availability if hardware exceeds its intended lifespan, making upgrades vital to meet regulatory requirements.

    Modern control systems not only support compliance but also enhance reliability, expand data collection and diagnostics, and reinforce system resilience, leading to safer, more predictable plant operations through improved visibility, redundancy, and health monitoring.

Customer stories, news & point of view articles

Explore our case studies to see how companies have successfully modernized their DCS and reaped the benefits:

Customer stories
Press releases
Feature articles

Resources

  • Contact us

    Submit your inquiry and we will contact you

    Contact us
Select region / language