Select Language
  • English
  • Deutsch

 

Test Documentation

All tests can be carried out as ABB tests or as PEHLA tests

 

 

Type Test Certificate


A type test certificate is issued for type tests which have successfully been carried out in full compliance with the relevant specifications or standards and STL Guides valid at the time of the test. For these tests the test object must be clearly identified by technical description, drawings and additional specifications.

Test Certificate


A test certificate is issued for parts of type tests which have successfully been carried out in full compliance with the relevant specifications or standards and STL Guides valid at the time of test. For these tests the test object must be clearly identified by technical description, drawings and additional specifications.

Test report


A test report is issued for all other tests which have been carried out according to specifications, standards or “PEHLA Richtlinien” (PEHLA Guides) and/or clients ‘instructions.
Similarly, this test report contains all test results, details of the conditions under which the tests were carried out, also details relating to the behavior of the test object, and its condition after the tests.

Test confirmation


A test confirmation is issued immediately after the tests. It confirms that the tests have been conducted and is valid only until publishing the detailed results in an entire document.

Contact

Phone: +49 (0) 2102 12-1477

E-Mail: testing@de.abb.com