ABB unveils an asset health solution optimizing switchgear efficiency

ABB improves switchgear efficiency and operational safety with ABB Ability™ Condition Monitoring for switchgear (SWICOM), reducing maintenance costs by as much as 30 percent.

ABB has unveiled a new asset health solution at Hannover Messe to optimize switchgear using real-time information of the electrical system, ABB Ability™ Condition Monitoring for switchgear - SWICOM.
ABB has unveiled a new asset health solution at Hannover Messe to optimize switchgear using real-time information of the electrical system, ABB Ability™ Condition Monitoring for switchgear - SWICOM.
center

With Industry 4.0, increasing focus is placed on the importance of monitoring and diagnostics to improve reliability and make the workplace safer. As a pioneering technology leader, ABB has unveiled a new asset health solution at Hannover Messe to optimize switchgear using real-time information of the electrical system, ABB Ability™ Condition Monitoring for switchgear - SWICOM.

Through monitoring and diagnostics of real-time information on the asset health of electrical systems, SWICOM lowers switchgear maintenance costs by up to 30 percent, prevents unexpected downtime by reducing failures throughout the power process and increases safety.

The consequences of revenue loss due to system failure can be substantial, especially in heavy industries. SWICOM helps to extend asset lifetime, and as a result increase the value of the electrical system investments for each installation.

“Condition monitoring increases availability and reliability of a primary and secondary distribution network, helping to identify a possible failure before it happens through a predictive approach,” said Alessandro Palin, Managing Director of ABB’s Distribution Solutions business line. “SWICOM supports optimizing of maintenance activities thus ensuring a maximal lifetime, also in case of severe ambient and operational conditions. And, as the switchgear condition is visible without having to open the panels, SWICOM concretely increases safety of personnel.”

Real-time data provides better support for decision making, allowing better analysis, optimization of operations and improvements in power quality. SWICOM allows site managers and operations managers to monitor the condition of their assets locally via a touch-screen human-machine interface and an intuitive mobile app. Connection with ABB Ability™ Asset Health for electrical systems – MyRemoteCare – enables visibility and tracking of the plant assets from anywhere in the world.

The solution is applicable to both ABB and OEM switchgear using IEC 61850-based protection. Having SWICOM installed on new switchgear saves time and effort for analyzing the switchgear condition. It provides a very cost-efficient solution as just one device supports a full lineup.

SWICOM also perfectly fits existing switchgear panels when the circuit breaker and protection relays are upgraded to IEC 61850 standard. It provides a scalable solution at a scalable cost – from essential monitoring to fully advanced prognostics, gathering data from the protection relays to additional temperature and partial discharge sensors.

Visit ABB’s booth at Hannover Messe, Hall 11, A35, to learn more about ABB’s smart, safe and sustainable offering.

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader with a comprehensive offering for digital industries. With a history of innovation spanning more than 130 years, ABB is today a leader in digital industries with four customer-focused, globally leading businesses: Electrification, Industrial Automation, Motion, and Robotics & Discrete Automation, supported by its common ABB Ability™ digital platform. ABB’s marketleading Power Grids business will be divested to Hitachi in 2020. ABB operates in more than 100 countries with about 147,000 employees.

Contact us

Share this article

Facebook LinkedIn X WhatsApp