ABB delivers total plant automation solution for Askari Cement in Pakistan

 ABB delivered a complete integrated ABB AbilityTM System 800xA centralized Distributed Control System (DCS) to upgrade the existing ABB Infi90 system

center

ABB in Pakistan recently completed a total plant automation solution for Askari Cement’s Nizampur plant in northern Pakistan. Askari Cement Limited is one of the leading manufacturers of cement in Pakistan. The company’s two plants produce cement used for construction of mega projects in the country including dams, bridges, highways, as well as commercial and industrial complexes and residential projects. The cement is also exported to India, South Africa and Afghanistan.

ABB delivered a complete integrated ABB AbilityTM System 800xA centralized Distributed Control Sys-tem (DCS) to upgrade the existing ABB Infi90 system as well as replacing all package third party PLC’s with ABB AC500 PLCs.

ABB has helped the plant operators at Askari Cement monitor their entire facility efficiently by providing a single dashboard and also installing the largest wireless network around the plant to connect all the products and systems reliably.

Most of the automation systems installed at the plant were at the end of their product lifecycle, lead-ing to maintenance issues for various third party Programmable Logic Controllers (PLCs).

“A centralized control system for the entire plant improves optimization, allows the customer to maintain a single system and helps in plant maintenance & operation,” said Zeeshan Ullah Chaudhary, project manager, ABB.

“ABB integrated all remote communication for distant areas within the cement plant over industrial wireless communication based on ABB TropOS technology, specifically designed for harsh environments with increased reliability. This has also reduced the cost for laying fiber optic cables. This project marks the first installed base of ABB TropOS system in the country,” he said.

Cement manufacturing is an energy-intensive process. Askari was keen to identify areas in its production line that need improvement in terms of energy usage. Through these process optimization solutions, the amount of energy used by Askari‘s production processes can be lowered and therefore made more efficient.

For instance, by making full use of ABB’s System 800xA capabilities, Askari‘s control room staff can adjust the process to run at its optimal level and reduce energy and raw material consumption, as well as keep vital processes running without interruption.

When an operator can use the integration of their process knowledge and System 800xA’s full capability, energy consumption can be reduced by 10%, explained Choudary.

The plant capacity here is 5,000 tons per day; for this project, the customer trusted our products and local service competencies, commitment to customer satisfaction and greater focus towards quality, he added.

“Pakistan’s infrastructure development is an integral part of our country’s growth,” said Najeeb Ahmad, Managing Director, Pakistan. “We contribute to the nation’s development by helping modernize factories as well as critical industries like cement.”

ABB (ABBN: SIX Swiss Ex) is a pioneering technology leader in electrification products, robotics and motion, industrial automation and power grids, serving customers in utilities, industry and transport & infrastructure globally. Continuing a history of innovation spanning more than 130 years, ABB today is writing the future of industrial digitalization with two clear value propositions: bringing electricity from any power plant to any plug and automating industries from natural resources to finished products. As title partner of Formula E, the fully electric international FIA motorsport class, ABB is pushing the boundaries of e-mobility to contribute to a sustainable future. ABB operates in more than 100 countries with about 135,000 employees. www.abb.com

Links

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp