ABB expands its offering for pulp measurements with L&W Crill

Add-on to fiber analyzers provides a complete range of fiber measurements, both image-based and non-image based, from one laboratory pulp sample for a truly holistic view of pulp fiber properties.

Zurich, Switzerland, June 27, 2016 -- ABB has launched the first laboratory fiber analyzer that has the capability to accurately detect the amount of crill in any pulp mixture. L&W Crill is an optional module to the portfolio of ABB's fiber analyzers. It uses a method based on the fact that small particles absorb and scatter light, which makes it possible to detect very small particles in a pulp suspension. It expands ABB's offering of Lorentzen & Wettre products for fiber testing.

Crill is an important variable to measure in pulp mixtures, as these tiny fibers contribute to overall paper strength and end product quality.

ABB's popular L&W Fiber Tester and L&W Fiber Tester Plus laboratory fiber analyzers are based on image analysis - there are more than 175 units installed worldwide. The addition of L&W Crill adds another dimension to pulp analysis and makes it possible to measure a new property.

L&W Crill analyzes pulp suspensions to monitor refining and dewatering. Refining the pulp increases the L&W Crill quota. During the refining process, the fibers are affected in different ways. For example, the fibrils of the fiber walls are exposed to a certain degree; these fibrillary particles on the fiber wall are described by crill. With this added capability, the L&W Fiber Tester Plus can now provide all information needed to understand pulp composition, including fiber length, fiber width, shape factor, fines content, fibril index and crill.

Because L&W Crill is not based on image analysis, it is not limited by the resolution of an imaging system. Instead, L&W Crill analyzes how particles with different diameters absorb and scatter light of different wave lengths. By sending UV-light and IR-light through a pulp suspension, it detects if small particles are present in the solution.

"We can now offer a complete range of fiber measurements methods within the same laboratory equipment, you can get a truly holistic view of your fibers from analyzing only one sample," says Anna Schärman, Global Product Manager, ABB AB/Lorentzen & Wettre products.

ABB (www.abb.com) is a leading global technology company in power and automation that enables utility, industry, and transport & infrastructure customers to improve their performance while lowering environmental impact. The ABB Group of companies operates in roughly 100 countries and employs about 135,000 people.

L&W Fiber Tester Plus - now available with L&W Crill, the option to measure crill.

Links

Contact us

Downloads

Share this article

Facebook LinkedIn Twitter WhatsApp