ABB technologies enable a stronger US power grid

ABB technologies enable a stronger US power grid

Innovative ABB solutions offer protection against extreme weather and physical attacks augmenting grid resiliency and enhancing power security

The impact of an extended power outage on an economy can never be underestimated. For insights, look no further than the cost of regional, weather-related outages such as major hurricanes in the United States alone.

In 2012, a Congressional Research Service study estimated the inflation-adjusted cost of weather-related outages at $25 to $70 billion annually. It is estimated that there were roughly 679 outages caused by weather events between 2003 and 2012, with the highest spike in years caused by superstorms like Hurricane Sandy. Thankfully, despite the increasing severity of such events, proper planning and quick reaction kept major outages confined, and power was restored to more than 95 percent of customers within days

As if natural disasters aren’t enough, there are also concerns related to physical attacks on power infrastructure with several instances in the last few years. The case for a more robust and resilient grid has never been stronger.

Aging infrastructure also makes the networks more susceptible to weather outages. In order to mitigate the impact of such events, electric grids needs to become more flexible, robust and allow a quicker response to outages through the use of technologies such as fault detection, isolation and restoration. Additionally, monitoring systems that perform complex functions, such as asset management, can greatly reduce capital costs and provide optimal grid efficiency.

Solutions include the use of software, sensors, asset management programs and a shift in the way industry professionals approach resiliency from traditional crisis planning to resiliency planning - preparing the grid ahead of time to prevent a crisis.

ABB has also launched the Substation Physical Security and Resiliency Initiative, which covers five strategic elements that will help utilities restore power as quickly as possible after an event that causes physical damage to a substation. These elements include Assessment, Hardening, Monitoring, Rapid repair and Rapid replacement. This initiative was conceived as a roadmap for any utility looking to develop solid disaster preparedness, response, and recovery plan, regardless of the type of physical disas-ter.

ABB has introduced the AssetShield™ ballistic protection system to protect transformers, meeting the UL-752 level 10 performance. AssetShield™is a first-of-its-kind solution that provides armor protection to large power transformers and other substation equipment from ballistic attack and reduces ‘spalling’ in case of impact. There is no visual difference between standard transformers and those with AssetShield protection, with the latter not requiring any additional maintenance or replacement measures.

ABB has won orders from three major US utilities for this innovative solution. The transformers supplied also feature Asset Shield tanks, dry bushings, impact sensors and automated cooling valves.

ABB’s TXtreme™ distribution transformer, which incorporates breakthrough technology designed to provide extra protection from harsh environments, can also help strengthen grid resilience. The unique coating, special processing and design criteria provide superior protection to distribution transformers so they can survive the elements and help reduce operations and maintenance costs because there is no longer a need to touch up or repaint the transformer due to corrosion. Additionally, TXtreme provides superior protection against leaks.

In another instance, ABB’s generator-circuit-breaker (GCB) technology is protecting key equipment in the iconic Hoover Dam to keep power flowing for people in Arizona, southern California, and southern Nevada. The GCB clears potential harmful short-circuit faults in tens of milliseconds preventing severe damages and possibly lengthy plant downtime.

The United States has over 200,000 miles of high-voltage transmission lines and thousands of substations and large electric power transformers. With operations including engineering, manufacturing and service locations throughout the country, ABB is committed to partnering with governments and utilities to protect the nation’s grid assets. 

Links:

Share this article

Facebook LinkedIn X WhatsApp