ABB’s DC fast charger is powering ComfortDelGro's first two fully electric cabs in under 30 minutes.
ComfortDelGro, one of the world’s largest land transport companies with operations in seven countries, has put two fully-electric Hyundai Ioniq taxis on trial in Singapore. The operator uses ABB’s Terra 53 DC fast charging station, and is available round-the-clock at Komoco Motors on Alexandra Road. Taking just under 30 minutes for a full charge, the Ioniq taxi can travel more than 200 km, and with ABB’s pioneering e-mobility technology the cost of charging it fully is only a third of the cost of diesel for the same distance.
Take a look at some of the photos from the launch event, to see how we are writing the future of smarter mobility:

ABB’s Terra 53 DC fast charging station at the Hyundai Motors showroom 
The two new fully-electric taxis during ComfortDelGro's launch event 
Johan de Villiers, Country Managing Director and Piera Man, Head of Corporate Communications, ABB Singapore, with Joseph Lim, one of the e-taxi drivers, at the ABB premises 
ABB is laying the foundation for a future of smarter, reliable, and emission-free mobility, accessible by everyone, everywhere 
With a view to expand and strengthen their partnership in e-mobility, Comfort Taxi has been offered free trial use of ABB's EV charger located at the office premises