ABB’s water-cooled motors deliver high efficiency in power-dense designs – see them at OTC 2023

ABB’s water-cooled motors deliver high efficiency in power-dense designs – see them at OTC 2023

  • Highly efficient - IE3-IE5 efficiency and bearing protection
  • High power density - 50% higher rating than similarly sized motors
  • Low maintenance - Water-jacket cooling eliminates fans and filters
  • See these and other ABB solutions at OTC2023, booth #1928

ABB will showcase its solutions for demanding process applications at the Offshore Technology Conference (OTC), May 1-4 at NRG Park in Houston, Texas, USA. Visit ABB at booth #1928.

ABB’s water-cooled motors represent a new generation of motor developed in response to market demands for improved technical features. Water-cooled motors are quiet, versatile and offer reduced maintenance and high performance in some of the toughest environments. Water-jacket cooling provides higher thermal conductivity than air cooling, helping to extend motor life while eliminating fans and air filters. Available with induction, synchronous reluctance (SynRM) or permanent magnet rotor technology, the motors can achieve high-efficiency (IE3-IE5) ratings for energy savings, and the power-dense designs deliver more power in a smaller footprint than similarly sized totally enclosed, fan-cooled motors. ABB’s water-cooled motors provide versatility for extreme marine, chemical, oil and gas applications, among others.

“High power and torque density means water-cooled motors provide superior performance in a compact size, and since the cooling is built into the frame, there is no need for extra space around the motors for air flow,” said Todd Huston, ABB’s global segment manager for process industries. “These motors are quieter than comparable air-cooled motors and can achieve a high level of efficiency. Water-cooled motors deliver more performance and lower overall operating costs in a smaller physical footprint compared to similarly powered motors of other designs.”

ABB’s water-cooled motors are available in four NEMA frame sizes from 60-1,250 Hp/45-932 kW (HydroCool XT) and IEC frame sizes 280-500 with ratings from 120-2700 Hp/90-2,000 kW (M3LP). Cooling efficiency is maintained even at low speeds, allowing for direct-on-line or variable-speed operation without derating or power loss - ideal for constant-torque applications. Shaft grounding is standard, and like most ABB products, the company’s water-cooled motors are equipped with provisions for ABB Ability™ Smart Sensor condition monitoring for instant motor health and performance information, providing connectivity and data analytics to make operations efficient, predictable and safe.

In addition to water-cooled motors, ABB will exhibit its top-drive drilling motors, IEEE 661XL, IEEE 841XL and IEEE 841 solid-shaft vertical P-base severe duty motors, the high-efficiency SynRM motor, ACS880 variable speed drive and ABB Ability Smart Sensor for condition monitoring.

ABB is a technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. The company’s solutions connect engineering know-how and software to optimize how things are manufactured, moved, powered and operated. Building on more than 130 years of excellence, ABB’s ~105,000 employees are committed to driving innovations that accelerate industrial transformation. www.abb.com

ABB Motion keeps the world turning – while saving energy every day. We innovate and push the boundaries of technology to enable the low-carbon future for customers, industries and societies. With our digitally enabled drives, motors and services our customers and partners achieve better performance, safety and reliability. We offer a combination of domain expertise and technology to deliver the optimum drive and motor solution ​for a wide range of applications in all industrial segments.​Through our global presence we are always close to serve our customers. Building on more than 130 years of cumulative experience​ in electric powertrains, we learn and​ improve every day. go.abb/motion

Contact us

Downloads

Share this article

Facebook LinkedIn X WhatsApp