- New expansion modules and software updates enable utility meter connection, blackout prevention, higher current measurement, customizable load prioritization and EV charger integration.
- InSite energy management system offers smart remote control and automation through digital motor operating and auto-reclosing devices to improve energy efficiency in any residential, commercial or industrial site
- Increased openness and interoperability through enhanced software capabilities and the ability to connect and integrate a greater number of devices
ABB has further extended its InSite smart energy and load management system, through new plug-in expansion modules, accessories, and software updates to improve energy efficiency in both sub and final distribution to enable additional use cases.
The InSite energy management system gathers data from field devices through the compact SCU200 central control unit. Plug-in expansion modules can be attached to the control unit to adapt the InSite system to various applications and requirements in sub and final distribution.
It provides energy transparency, remote monitoring, and predictive maintenance with real-time data accessed via a user-friendly InSite web server dashboard or third-party application. InSite energy management system can be scaled from large buildings to homes and enables users to optimize energy usage and achieve full load management, easily integrating electric vehicle (EV) chargers, photovoltaic (PV) systems, utility meters, and more.

InSite Energy management system 
InSite Energy management system
New enhancements to the InSite system include a plug-in USB module that, among other functions, enables connection to utility meters and the software update. This provides a greater level of energy monitoring as well as blackout prevention through the ability to adjust or schedule consumption such as reducing or pausing EV charging sessions.
The new energy meter module can now measure higher currents while an added smart auxiliary and signaling contact can read the on and off status of devices for critical applications in hospitals or data centers so that action can be taken in the event of a trip.
Sebastiano Paganini, Global Product Line Manager for Energy Management Solutions at ABB Electrification’s Smart Buildings division said, "As the InSite system expands, it becomes even more scalable and flexible. We have collaborated with customers to understand and develop additional modules and device integrations to meet their specific requirements. These include EV chargers and utility meters. A wider variety of loads can be monitored and controlled, improving load management capabilities and energy efficiency."

InSite Energy management system architecture 
InSite Energy management system components overview
In addition, new smart accessories and a new series of power meters have been released and can be connected to InSite:
- Motor operating devices allow the remote control of the coupled devices and can also be connected to InSite so that they can be switched on and off remotely via the InSite web server directly or through set automations.
- Auto-reclosing devices automatically switch coupled devices back on in the event of an unwanted trip to ensure continuous operation of systems and appliances, such as refrigerators. For example, if a Miniature Circuit Breaker (MCB) trips, the Auto-reclosing device will attempt to reset the tripped MCB following a temporary fault or blackout. Integration with the InSite system enables users to receive alerts for recurring faults and monitor all activity via the InSite web server.
- D1M power meters monitor energy usage of devices connected to InSite and provide energy flow analysis covering comprehensive measurements and full metering capabilities to improve the energy efficiency of the electrical system for any standard application from buildings to industries.
Third-party devices and appliances can be integrated for balancing energy availability and demand to enable customized prioritization of loads. For example, with the new EV charger integration functions, you can choose between time-optimized or energy-efficient charging, maximizing the use of self-generated electricity by prioritizing solar energy over grid power.
ABB is a technology leader in electrification and automation, enabling a more sustainable and resource-efficient future. The company’s solutions connect engineering know-how and software to optimize how things are manufactured, moved, powered and operated. Building on over 140 years of excellence, ABB’s more than 105,000 employees are committed to driving innovations that accelerate industrial transformation. www.abb.com
ABB Electrification is a global technology leader making efficient and reliable use of electricity from source to socket possible. With more than 50,000 employees across 100 countries, we collaborate with our customers and partners to solve the world’s greatest challenges in electrical distribution and energy management. We help businesses, industry, and consumers run their facilities and homes efficiently and reliably. As the energy transition accelerates, we are electrifying the world in a safe, smart and sustainable way. go.abb/electrification